1/5/2025 6:16 PM | |
Joined: 10/5/2016 Last visit: 8/10/2025 Posts: 109 Rating:
|
Hi Murof, https://support.industry.siemens.com/forum/ae/en/posts/two-single-user-project-and-future-engineering-station/279731 As per in the above post, in the case we have a simatic manager, is it best to import the single station OS into the simatic manager and then perform the changes and do download from simatic manager. Could you please also tell whether by doing this way that the archive data will not be lost. We also have 1 ES( Step7 5.5SP2 and Wincc RC 7.4) and two single station OWS.( Wincc RT 8.0 ). This is a existing running plant and we are looking to add one more ET200M IO rack and also changing the CPU from S7300 to S7400 Also since there is a change in the version of RC 7.4 and RT 8.0 , we are looking to upgrade with minimum changes to the system. ( Instead of integrated whether doing the changes on the RT with the 2hr free window provided is a simple way to do Wincc engineering on RT station itself because if we want to upgrade RC to 8.0 , then the Windows EWS OS which is now Windows 7 has to be changed to Windows 11 and all the software in the EWS has to be upgraded which may be a tedious task) ------------------------------------------------------------------------------------------ |
Last edited by: arunvt1992 at: 01/05/2025 18:18:06Last edited by: arunvt1992 at: 01/05/2025 18:22:03Last edited by: arunvt1992 at: 01/05/2025 18:22:50Last edited by: arunvt1992 at: 01/06/2025 07:10:30Last edited by: Moderator_Lan at: 01/07/2025 08:42:37New subject after splitting |
|
1/9/2025 10:27 AM | |
Joined: 8/3/2009 Last visit: 9/12/2025 Posts: 16409 Rating:
|
Hello arunvt1992 It is not necessary to have an integrated WinCC Project in Simatic Manger. It is needed only if you use special Configuration like a redundant server pair and you want to do online delta loading to both partners for example. Just to keep the RT Data you can also use a workaround like this: https://support.industry.siemens.com/cs/de/en/view/24193864 Also keep in mind that WinCC Version on every Server, Client and ES has to be the exact same version (also same Update!) Perhaps this FAQ already helps in your situation, If not , or if I misunderstood your usecase, please leave also a comment Bye Murof |
Last edited by: Murof at: 01/09/2025 10:30:35If this Information really helps, you could use the Rate function |
|
Follow us on