3/27/2025 9:22 AM | |
Joined: 8/3/2009 Last visit: 9/12/2025 Posts: 16409 Rating:
|
Hello AutoGen_1260505 just to clarify and understand your usecase... You have a Faceplate instance in your screen. On this object you have set your properties. If you click on the Faceplate instance in RT you want to open a Popup Screen with another faceplate and in this faceplate popup you use the same properties/tags? In this case you should be able to use the interface informatoin and tags also for the popup. Check this manual information: https://support.industry.siemens.com/cs/ww/en/view/109976850/182731414667 Bye Murof |
If this Information really helps, you could use the Rate function |
|
3/31/2025 8:39 AM | |
Joined: 11/7/2019 Last visit: 8/28/2025 Posts: 21 Rating:
|
Yes, but I want to retrieve the properties (User defined properties) and not the tags. Is this possible? |
Follow us on