4/22/2025 4:48 PM | |
Joined: 5/24/2016 Last visit: 9/11/2025 Posts: 412 Rating:
|
Hello. So eventhough it is specified as a S7-1500 the PLC does not have all the same features and functions as a "regular" S7-1500. And I am speculating as to your application, but i believe in general what you are trying to achieve is not possible. If you want to use them as pure position axis, you need to configure and license them as such. please look on page 281 on this manual - Sinumerik ONE - Axes and spindles Best Regards Riddersholm |
This contribution was helpful to
1 thankful Users |
4/24/2025 5:06 AM | |
Joined: 8/4/2012 Last visit: 5/15/2025 Posts: 4 Rating:
|
I created the drive configuration with Drive In-bult Positioning and used the SINAMICS Positioning Technology Object to get the required customer functionality. Thanks. |
Follow us on