5/6/2025 10:54 AM | |
Joined: 3/17/2023 Last visit: 7/21/2025 Posts: 1 Rating:
|
Hi I am working on an app to help me untangle the action log into a more visual way an i was wondering if there was a way to increase the Action LOG size. After looking around i found that the default size is 5 MB (I manage to find it for the 828D, I am interested in the 840 and One but I suppose the size is the sameSINUMERIK 828D: Activate and save action log - ID: 58692255 - Industry Support Siemens) And testing corroborates it. Looking at the parameters I though maybe The 18374 MM_PROTOC_FILE_BUFFER_SIZE was the limiting one but after testing in sinutrain it does not seem to be the case. I was wondering, is there any way to increase the size/length of the action log. And if such, how. |
Last edited by: Moderator_Lan at: 05/06/2025 11:51:31link optimized |
|
Follow us on