6/4/2025 4:52 AM | |
Joined: 3/14/2008 Last visit: 9/11/2025 Posts: 2216 Rating:
|
Hi, That's unfortunate! I think the only remedy is to try to execute a readback and hope it will succeed so that you have at least all OCM variables saved in the offline CFC program. If you have user DB's it's also wise to upload the online db's to an empty S7_program (Link) so you can check. And then a full download of the AS is necessary.
|
Last edited by: Moderator_Lan at: 06/04/2025 06:49:17link optimized If I could help you, you can use the RATE button. Thank you. |
|
Follow us on