6/25/2025 7:29 AM | |
Posts: 1 Rating:
|
To store the data recorded by the HMI, I need to install an external hard drive in the USB port. Is there a specific model that should be used? |
6/25/2025 12:23 PM | |
Joined: 7/5/2013 Last visit: 9/10/2025 Posts: 3241 Rating:
|
Hi, you may find further information in the following FAQ [especiallly section 3) Information]: Which external storage media can you use with the current SIMATIC panels and which memory card interfaces do they have? Regards, Frink |
Pi is exactly three! |
|
Follow us on