8/6/2025 5:35 AM | |
Joined: 12/18/2014 Last visit: 9/17/2025 Posts: 35966 Rating:
|
Firmware updates and OSS information for the system SENTRON COMThe newest firmware version of the SENTRON circuit breakers with measurement and communication is provided here. Firmware Updates of the SENTRON COM circuit breakers with measurement and communication. We recommend the latest version of the commissioning and service software powerconfig 63452759 All SENTRON COM devices are updated together via one file. This firmware (FW) file is transferred tothe 7KN Powercenter 1000 or 1100.
|
This contribution was helpful to
1 thankful Users |
Follow us on