8/25/2025 1:36 PM | |
Joined: 7/11/2022 Last visit: 8/25/2025 Posts: 56 Rating:
|
Hi, |
8/27/2025 7:07 AM | |
Joined: 9/2/2024 Last visit: 8/28/2025 Posts: 40 Rating:
|
Hi, have you correctly configured the settings in the Set PG/PC interface? |
8/29/2025 6:45 AM | |
Joined: 8/3/2009 Last visit: 9/5/2025 Posts: 16343 Rating:
|
Hello Hero_ac Even if you have deactivated the Secure HMI communication in the PLC you MUST use the scada Export tool !!!!!! It will not work if you do not use it at least to import the certificate. It is easy to keep in mind, if you have WinCC V7.5SP2 Upd4 or newer, then you MUST use the SCADA Export tool to get the Certificate. It is a must, and it do not depend if you have activated the Secure HMI communication or not. Also habe a look in the Channel Diagnosis Tool on WinCC while RT is running, perhaps you find a few more detail information also. Accesspoint in Channel Configuration has to be correct and in PGPC Interface you have to set this Access Point to your networkcard.TCPIP.1 Have also a look at this FAQ: https://support.industry.siemens.com/cs/de/en/view/101908495 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on