8/26/2009 11:39 AM | |
Posts: 10 Rating:
|
Dear all i want to convert this pieace of S5 instruction to S7 which contain LIR1 : FB234 nom :DASA Design EQNR E BY L =EQNR B MW 196 A DB 0 L DW 9 TAK < F BEB L DW8 : F T MD 250 L DW6 +F LIR1 ......... As I Know to convert LIR1 i must have value of accumulateur1 which is the conserned adress so LIR1 is replaced by the value of this adress. but using only the programm and i know that the plc is related to an old op 3XX ,how can i resolve this problem?? (i think that i have to know the realtime value of (mw196,dw9,dw8,dw6) which is only possible if i am near the PLC????) for more details i attached the plc program. thnaks and best regards. AttachmentBEJA42ST.zip (408 Downloads) |
Follow us on