3/9/2010 4:36 PM | |
Joined: 6/4/2008 Last visit: 8/5/2025 Posts: 1518 Rating:
|
Hi, the part number for the IGBT is BSM400GA120 DN2S. The ideal way to test an IGBT is to run it under load, however, it is possible to test it at 24VDC. Using the Masterdrive testbox is one way (6SE7090-0XX84-1FK0) Please see the attached documents for testing IGBT's and SCR's (Rectifiers) with meters, maybe they can help you. Cheers, Graeme AttachmentIGBT_&_SCR_Testing.zip (358 Downloads) |
Follow us on