5/18/2010 11:14 AM | ||||||||||||||||
Joined: 8/10/2005 Last visit: 4/9/2024 Posts: 1486 Rating:
|
Import of a Technical Reply of an User UMENCHO wrote: Hello, To clarify situation. To connect MIDI Master drive with PC you need RS232/RS485 converter. There is a 9-pin SUB-D socket connector (X502) on the membrane keypad which provides access to the RS 485 interface. Pins assigment you could find in http://automation-drives.ru/sd/download/archive/3/da64_en.pdf page 67. Another way (seems you have it) with optional Clear Text Display. Its provide isolated RS232 interface for connecting to a PC. Description of pins find in How to download from old thread.Now if we assume cables and "drive' are ok this failure could be regard to COM port of PC. Check there settings of COM port. My suggestion is:
Hope this will helps. Best regards, Hristo Mihalev |
|||||||||||||||
Follow us on