9/24/2010 5:31 AM | |
Joined: 8/25/2006 Last visit: 9/10/2025 Posts: 2218 Rating:
|
Hello. Here is the manual about how to use SIMOREG for DC-Motor Generator Set Control. In the main manual for Simoreg you may read about computation cycles in chapter 9.2, and for S00 blocks in chapter 8 sheet B101. Minimum cycle time that is used for function calculation in Simoreg isT0 = 3.33 ms at 50 Hz line frequency or T0 = 2.78 ms at 60 Hz line frequency. In your application main control loops will be calculated in this cycle time. |
Follow us on