10/29/2010 9:12 AM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Dear MeGo, Do you find the .FWX file. Did the compilation complete without errors. (See Output view) Are the WinCC flexible version of Configuration PC the same as on visualization PC? Perhaps this link might help: Which settings must you make on the RT Loader to transfer a WinCC flexible Runtime file from the configuration computer to a visualization PC? Best regards, Wizard |
Follow us on