10/31/2010 12:24 PM | |
Joined: 7/28/2010 Last visit: 8/31/2024 Posts: 184 Rating:
|
Bee, Open Winccflex. Go under Project/Communication/Connection. Checkparameters for"Connection_1", it should have the right profibus addresses.as you have setup. Regards, Behnam www.sigmaprocess.ca |
11/2/2010 11:28 AM | |
Joined: 4/24/2006 Last visit: 9/15/2025 Posts: 9027 Rating:
|
Dear SpaceBee, Have you tried to start Runtime in stead of Simulator? Perhaps these links might help: how do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS?MPI? Best regards, Wizard |
11/2/2010 12:07 PM | |
Joined: 7/28/2010 Last visit: 8/31/2024 Posts: 184 Rating:
|
Bee, You have mentioned that your I/O field is set to Output. This will not pass your value to CPU. Set it either to "Input" or "Input/Output". Regards, Behnam www.sigmaprocess.ca |
This contribution was helpful to
1 thankful Users |
11/2/2010 9:05 PM | |
Joined: 9/27/2006 Last visit: 9/16/2025 Posts: 12409 Rating:
|
Hello SpaceBee; Congratulations on setting up your first working tags in WinCC Flexible. Have you thought of interating your WinCC Flexible program in your Step 7 project? It would relieve you from the task of creating each tag in WinCC flexible based on the I/O address in the PLC by hand, amongst other things. Have a look at the following link: How do you integrate a WinCC flexible project in STEP 7? And search for "integration" in the WinCC Flexible online help. Hope this helps, Daniel Chartier |
Follow us on