11/6/2010 2:26 PM | |
Posts: 141 Rating:
|
The version of WinCC project I have in computer is not the same as the one in OP. I would like to synchronise them, but since as far as I know its not possible to decompile it, I had to add features that are missing to my old project. So, in order that this be as painless as possible, I would like to backup somehow WinCC project that is currently in OP, then after I can download mine, and see if it is working correclty or not. And if it is not working correctly, to be able to safely retyrned the backuped version from OP. In order to backup current software in OP, can I just do copy/paste, or I need to do something else also? [schnippschnapp] second question is splitted to how to replace one version of WinCC flexible project with another version in Step 7?. Thanks, Goran |
Last edited by: O_Moderator at: 11/8/2010 11:25 AM |
|
Follow us on