2/11/2011 4:40 PM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello, Is the "Transfer" grayed out or not available? Is the problem only in this project? Try to do the following: in WinCC flexible -> Options -> Delete temporary files Then compile the project again. In Step 7, save your project with "Save As" and the option "With reorganization slow" selected. Or perhaps this link: how can you reset WinCC flexible to the original status of the last installation? Best regards, Wizard |
Follow us on