5/6/2011 10:26 AM | |
Joined: 12/1/2006 Last visit: 7/10/2025 Posts: 26 Rating:
|
Doing a simulation of the car. WinCC flexible Runtime is running a simulation of the car, brake or clutch pedal is pressed from the outside in WinCC Runtime want to play the appropriate sound. When pressed a button in WinCC Runtime running the sound I know. However, depending on the audio file does not work with an external switch. I wrote the script works, but once running. Page after you install the brake pedal is pressed the script does not work AttachmentDesktop.zip (98 Downloads) |
5/6/2011 12:01 PM | |
Joined: 9/1/2005 Last visit: 8/22/2025 Posts: 4114 Rating:
|
closed cause question posted twice. The second thread with the subject MP3 is published within the same conference. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on