5/23/2011 10:33 AM | |
Joined: 10/7/2010 Last visit: 7/25/2025 Posts: 103 Rating:
|
Hi is possible to get the ip address of panel on wincc flexible? I'm using a MP377 12" touch - color thx in advance |
5/23/2011 10:44 AM | |
Joined: 4/29/2010 Last visit: 1/20/2025 Posts: 1557 Rating:
|
Hello, i think you mean a solution without going to the control panel and check the ip-settings? best regards |
5/23/2011 12:33 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello, I think this is not possible directly. Each panle exchange data with CPU. In way how you detect the network connected with each panel, assign one specific tag which will show a message in WinCC Flex that this panel has IP192.16... Take a look at How can you share runtime-generated parameters between several S7-1200 PLCs with a KTP Basic Panel? .This FAQ is not concerning directly yoyr issue but might ne given you some ideas... Best regards, Hristo Mihalev |
Follow us on