6/24/2011 8:27 AM | |
Posts: 40 Rating:
|
hi everyone when i load the project to the panel i am getting a error which is on attachment please help thanx in advance |
6/24/2011 8:34 AM | |
Posts: 40 Rating:
|
hi eventhough i contuniue yes or no loading is interrupting so what should i do ? |
6/24/2011 8:34 AM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello, Did you try with Yes? Or did you asked what exatly is it meaning? What is the type of panel? Make it a reset to factory settings using http://support.automation.siemens.com/WW/view/en/19701610 Best regards, Hristo Mihalev |
Last edited by: UMENCHO at: 6/24/2011 8:41 AM |
|
6/24/2011 8:36 AM | |
Posts: 40 Rating:
|
i tried both yes and no but happens an interruping |
6/24/2011 8:59 AM | |
Posts: 40 Rating:
|
hi i attached output i am using tp177a 6 inch |
6/24/2011 9:37 AM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Dear niila, How do you want to transfer project to Panel? What type of cable you use? Have a look at the following links: how can you transfer a WinCC flexible project serially to a panel? how can you transfer a WinCC flexible project via MPI/PROFIBUS to a Windows-based panel? Best regards, Wizard |
6/24/2011 3:56 PM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello, Have a look at this link: What transfer options are available in the various operator panels? Are you using USB PC adapter (6ES7 972-0CB20-0XA0) Best regards, Wizard |
Follow us on