6/23/2011 9:11 AM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello, Check it there http://support.automation.siemens.com/WW/view/en/19109408 Best regards, Hristo MIhalev |
This contribution was helpful to
1 thankful Users |
6/23/2011 9:29 AM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello, Perhaps this link might help: how can you transfer a WinCC flexible project via MPI/PROFIBUS to a Windows-based panel? Best regards, Wizard |
This contribution was helpful to
1 thankful Users |
6/25/2011 9:20 AM | |||
Joined: 2/1/2011 Last visit: 7/27/2025 Posts: 14 Rating:
|
According to below detalis, can i transfer or download My project to panel KTP1000 Basic DP? My devices are:
http://support.automation.siemens.com/WW/view/en/19109408 Notes on the USB PC adapter (6ES7972-0CB20-0XA0) The USB PC adapter provides an MPI/DP interface via the PC's USB interface. More information is available in the manual in Entry ID: 16983464. This cable is released only for the devices below for project transfer and OS updating.
|
||
6/26/2011 9:17 AM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Should it be possible. Did you try it? Best regards, Hristo Mihalev |
6/26/2011 1:58 PM | |
Joined: 2/1/2011 Last visit: 7/27/2025 Posts: 14 Rating:
|
yes, I do. but do not transfer my project to panel. |
Follow us on