8/11/2011 9:28 PM | |
Posts: 5 Rating:
|
Hello, I have a Windows based operating panel MP277 10" touch and a CPU 313C. I want the clock of the OPin my CPU because after a few weeks the time op the CPU is not correct. I found a tutorial on the siemens support https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objId=36043317&load=treecontent&lang=en&siteid=cseus&aktprim=0&objaction=csview&extranet=standard&viewreg=WW but when I do this the CPU clock gets in my OP and I want the opposite. I do part 2.2 of the tutorial. Can anyone tell me what I do wrong. I use winCC flexible 2008 SP2 en Step 7 5.5 Thanks for the help Ruben |
8/12/2011 4:54 PM | |
Posts: 5 Rating:
|
Hello, Thanks for the reply, I took a print screen of the area pointer screen Ruben |
8/15/2011 8:47 AM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating:
|
Hi, which of the Address did you use => DB101.DBWW10 or DB101.DBW22? For what did you use the DB101,DBW22? regards, |
8/16/2011 12:18 PM | |
Posts: 5 Rating:
|
Hello, I imported the files from te attachment in my step 7 project, but do I have to configure settings in the db to get this work? kind regards Ruben |
Follow us on