8/19/2011 10:20 AM | |
Posts: 8 Rating:
|
hello i write this simple project with step 7 v7.5.(on and off motor) and then create a hmi station. my problem is that when i run wincc flex simulator and change the variable nothing change.(for example: when turn on i0.0 in plcsim nothing change in wincc simulator page and when push the button in wincc flex nothing change in plcsim ) i work 3 days on the problem.(such as check the tag and connection).but now i give up. i cant find the problem. i attach the project .please some one download it and tell me what is wrong? thanks AttachmentTest2.zip (196 Downloads) |
8/19/2011 6:09 PM | |
Posts: 8 Rating:
|
please someone upload a project that on and off a motor and be controlled with plcsim i always pray for you. it is for a week im working on it but couldnt do it. |
8/19/2011 6:27 PM | |
Joined: 1/28/2009 Last visit: 8/31/2025 Posts: 6874 Rating:
|
Hi Check the attachment Regards AttachmentPUMP.zip (195 Downloads) |
This contribution was helpful to
1 thankful Users |
8/20/2011 2:00 PM | |
Posts: 8 Rating:
|
im still waitting please |
8/20/2011 11:37 PM | |
Joined: 10/7/2005 Last visit: 9/4/2025 Posts: 3049 Rating:
|
Hello tak2750 while youwait for someone to do your work for you, allow to make a few other suggestions in the meantime: 1.) There's a fair few example WinCC flexible projects available from Siemens, do a search at https://support.automation.siemens.comand also check the Applications & Tools section, you'll be suprised what you can find. 2.) You say that "...i run wincc flex simulator". Could it bethat you indeed click on the "Start Runtime with Simulator" icon (the icon that shows an arrow pointing to the bottom right hand corner)? If so, this option is designed to test your HMI without a PLC (or S7 PLCSIM) and you won'tget a connection to S7 PLCSIM. Usethe "Start Runtime system" icon instead (the icon that looks like a PC) to get a connection to S7 PLCSIM. I hope this helps |
Cheers |
|
This contribution was helpful to
1 thankful Users |
8/21/2011 9:48 AM | |
Posts: 8 Rating:
|
thanks a lot. that was the problem. that help me. thanks again |
This contribution was helpful to
1 thankful Users |
Follow us on