10/10/2011 8:53 PM | |
Posts: 4 Rating:
|
If this is possible via industrial ethernet how can I access single S7-300 through two PC\ |
10/10/2011 10:06 PM | |
Joined: 5/28/2008 Last visit: 9/3/2025 Posts: 4522 Rating:
|
Hello,
Hope this helps. |
Ayman Elotaify |
|
10/12/2011 11:40 AM | |
Posts: 4 Rating:
|
|
10/13/2011 4:29 PM | |
Joined: 5/28/2008 Last visit: 9/3/2025 Posts: 4522 Rating:
|
You are welcome.
|
Ayman Elotaify |
|
10/14/2011 7:22 AM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
How do you configure a connection between WinCC flexible Runtime (PC or Panel) and a SIMATIC S7-300 / S7-400 via Industrial Ethernet? How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI? Take in mind Which connection resources are occupied in the S7-300 CPU for communication connections and services of the Industrial Ethernet CP? and How do you parameterize the communication resources of S7-300 CPUs so that WinCC stations and S7-300 stations do not have connection failures? in case of ethernet connection. And in case of Profibus Does PROFIBUS DP communication use connection resources? Best regards, Hristo Mihalev |
This contribution was helpful to
1 thankful Users |
Follow us on