2/23/2012 4:10 PM | |
Posts: 739 Rating:
|
Hi, To reset all parameters to the factory default settings; the following parameters should be set as follows: Set P0010 = 30 Set P0970 = 1 P970 = 3 is not possible. But therer are (see attached): P1910 Select motor data identification = 2 P1960 Speed control optimisation = 3 and do not forget to set P3900 = End of quick commissioning! to set the comand / setpoint sources: p1000 = Setpoint source p0700 = Command source AttachmentQuick-commissioning_en.pdf (192 Downloads) |
Follow us on