3/26/2007 6:55 PM | |
Posts: 7 Rating:
|
Hello , I desired to connect a scanner of “Barre Codes” on a connection RS232C on a CPU314+CP340 (6ES7 340-1AH01-0EAE0) I would like to know if there is a sample program with the FB4 (P_Print) so yes? or then I to download it? thank you My Scanner has code bars functions trés under WindowsXP with “HyperTerminal” on Com1 (Series). But I recoit nothing in the DBxx which I have to configure, if I connect it on the Chart of the automat, have ideas thank you in advance for your answer. AttachmentSG_1160_bt-schluessel.pdf (471 Downloads) |
Follow us on