7/5/2012 8:23 AM | |
Posts: 95 Rating:
|
Picture is here |
7/5/2012 10:48 AM | |
Posts: 3037 Rating:
|
Hello AlecTek, The cycle time is always greater as the HMI Enable Time at WinAC MP. Cycle Time = OB1 execution time + HMI Enable Time You can find more information about HMI Enable Time in the following manual on the chapter 5.3.8. SIMATIC WinAC MP 2008 The default of HMI Enable Time is 50 ms. You must check screen change and refresh time during operation of the panel. You can decrease the HMI Enable Time, if the screen change and refresh time during operation of the panel is ok. See the chapter 5.3.9. Tweety |
This contribution was helpful to
1 thankful Users |
Follow us on