7/6/2012 2:12 PM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello joemckibben, Please have a look at the following link: What transfer options are available in the various operator panels? and how can you transfer a WinCC flexible project serially to a panel? Best regards, Wizard |
7/6/2012 2:39 PM | |
Posts: 3 Rating:
|
Ok thanks for the info Wizard. Just to make sure I understand correctly, I can use RS-232 I just need to use a laptop that has a com port on it?
|
7/6/2012 3:23 PM | |
Posts: 3 Rating:
|
But would a USB/MPI cable be my best option? Are they all the same? Or will any do? I didn't see an actual part# for one. |
7/6/2012 3:39 PM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello, Have a look here: how can you transfer a WinCC flexible project via MPI/PROFIBUS to a Windows-based panel? first note: PC-adapter (USB or RS232) are not supported. Although it sometimes does work. Best regards, Wizard |
7/6/2012 5:23 PM | |
Posts: 8946 Rating:
|
Hello Wizard, I can confirm that it works with KTP panels all the time. |
This contribution was helpful to
1 thankful Users |
Follow us on