8/7/2012 1:00 PM | |
Posts: 8 Rating:
|
Respected Sir, We are using WinCC Flexible PC as Run time option. We have been trying to send email through sm@rt server on alarms, we have gone through the manuals but the following points are still not clear- 1. Server Name- Which server name has to be given, if we are using modem or else normal official mailoutgoing server. 2. Email Address- Which email address do we have to write? Can we use any gmail address or do we have to use official mail id linked with official ouitgoing mail server. 3. Login- Which login id has to be written? 4. Password- Does it have to be the password of the senders email id? I am attaching the bmp of the device settings iI have done in Winc flex and also the print screen of the error I get. Kindly suggest if any modification has to be done or any other setting has to be done. Thanks & Regards Attachmentattachment.zip (123 Downloads) |
8/7/2012 3:53 PM | |
Posts: 3037 Rating:
|
Hello plc..., youshould followthe description about email sending in the following link. How do you send e-mails from a Windows CE panel or PC with SIMATIC WinCC flexible? Tweety |
Follow us on