10/16/2012 2:42 PM | |
Posts: 3037 Rating:
|
Hello Urantia, You can use the function "Rebuild All" in WinCC flexible. Then you transfer the project new. You see a message "the project download is successful"in the Output Window of WinCC flexible. Or you do an OSUpdate. How do you do an operating system update (OS update) on operator panels? Then you do a project download. Tweety |
10/16/2012 2:47 PM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello Urantia, You can not be sure it is the same project. I would suggest to first backup the project from panel, so you can always go back to old situation. how do you backup/restore with a Windows-based panel? Best regards, Wizard |
Follow us on