4/16/2013 7:44 AM | |
Joined: 9/2/2012 Last visit: 6/3/2019 Posts: 176 Rating:
|
Hi, We have a IPC277D nano-panelpc, with Windows XP Embeded (default install), after the installation of the wincc RT with license that was suggested to be used together in my previous thread doesnt seem to work with the suggested WinCC-version. First of all, we cannot select IPC277D as panel in the wincc device settings and we have to use Panel PC as option, selecting version 1.4.0.0 (as seen on picture 9F97AnY.png in attachment) The installed software is: Products: QenoAtP.png in attachment WinCC: n13bcq4.png in attachment On the panel we start the WinCC loader and select transfer after settings has enabled Ethernet and remote control. This is the transfer-log from WinCC from pictures above:
14:04:25.04 Compiler Info : Compiling started ... 14:04:25.57 Compiler Info : Linking target 'Device_1' ... 14:04:25.57 Compiler Info : Number of generated tags: 139. 14:04:25.57 Compiler Info : Number of PowerTags used: 87 14:04:25.59 Compiler Info : Required license: WinCC flexible /Recipes for PC-RT 14:04:25.59 Compiler Info : Succeeded with 0 error(s), 0 warning(s). 14:04:25.59 Compiler Info : Time stamp: 2013-04-15 14:00 - used 285060 bytes 14:04:25.59 Compiler Info : Compiling finished! 14:04:25.59 Transfer Info : Starting transfer for Device_1 14:04:25.59 Transfer Info : Checking version on target device ... 14:04:25.59 Transfer Info : Transferring project ... 14:04:25.59 Transfer Info : Transferring Device_1 (WinCC flexible Runtime) 14:04:28.04 Transfer Info : Establishing connection to device... 14:04:29.54 Transfer Info : Download is not possible. This WinCC flexible ES version and the WinCC flexible Runtime software version on the operating unit are not compatible. 14:04:29.54 Transfer Info : Transfer failed! Attachmentpictures.zip (145 Downloads) |
Last edited by: O_Moderator at: 4/18/2013 9:08 AMpictures transferred to attachment |
|
4/17/2013 11:43 AM | |
Posts: 3037 Rating:
|
Hello FuriousRage, Haveyou installed the Runtime of WinCC flexible 2008 SP3 on the Panel PC? Tweety |
This contribution was helpful to
1 thankful Users |
4/17/2013 1:49 PM | |
Posts: 54 Rating:
|
doesn't it also say you need a recipe license |
Follow us on