6/3/2013 12:38 PM | |
Joined: 9/27/2006 Last visit: 9/18/2025 Posts: 12414 Rating:
|
Hello iservos; Siemens is a huge worldwide company with many different divisions, each specialized in certain technologies. This forum is maintained by the Siemens Industrial Automation and Drives division. Most of the participating members here do not work directly with telephony, even with Siemens products. Possibly someone here will have experience with the products you are asking about, but do not feel left out if you get no direct answers from the forum. There are however many links on the web on the HG 1500 I can only suggest you examine them to see if you will find your own answers: http://www.google.ca/#output=search&sclient=psy-ab&q=+number+of+licensed+B+channels+for+HG+1500+V3.0&oq=+number+of+licensed+B+channels+for+HG+1500+V3.0&gs_l=hp.12...1598.1598.0.5870.1.1.0.0.0.0.95.95.1.1.0...0.0...1c.1.15.psy-ab.w1D10OL2lXI&pbx=1&bav=on.2,or.r_qf.&bvm=bv.47244034,d.dmg&fp=d3be08f6e5f2d5a0&biw=1537&bih=770 Hope this helps, Daniel Chartier |
Follow us on