(0)| 6/15/2013 10:20 AM | |
|
Posts: 1064 Rating:
|
Your drawing looks good and should work as for the pac3200 sorry but i can't help you there nas i have never worked with them |
| 6/17/2013 4:24 AM | |
|
Posts: 1064 Rating:
|
try in low voltage forum they should be able to help |
| 6/17/2013 4:58 AM | |
|
Joined: 9/27/2006 Last visit: 1/13/2026 Posts: 12480 Rating:
|
Hello Raffy; Based on the followingFAQ, there seems to be more than simply importing the gsd file and setting up the network hardware to configure the PAC 3200 as a Profibus-DP slave: Unable to establish a connection between SENTRON PAC3200 and S7 PLC via Profibus DP "Detailed information about configuration of GSD file is given in the manual SENTRON Expansion module PAC PROFIBUS DP „Chapter 6.4 Configuring by means of the GSD file" A link to the manual is presented in the FAQ. Please show us the steps you have done up to now. Hope this helps, Daniel Chartier |
This contribution was helpful to
|
|
Follow us on