6/24/2013 10:12 AM | |
Posts: 515 Rating:
|
Hi, Refer the below attachment. It is used for TIA but the procedure is same for wincc flexible too. First assign an ip address for the simatic panel, assign an ip for the plc too(both the ip's should fall under the same network id) and then configure these IP adresses in the connections of the wincc flexible software. it should just simply work
AttachmentWinCC_TIA_Portal_Ethernet_Transfer_en.pdf (239 Downloads) |
6/28/2013 10:11 AM | |
Posts: 3037 Rating:
|
Hello, You use a Panel PC with Runtime, then you use the CP "IE-gerneral". See the following link chapter 1.2 http://support.automation.siemens.com/WW/view/en/24109937 The CP "HMI-IE" is for Panel with WinCE. Tweety |
Follow us on