9/23/2014 11:30 AM | |
Posts: 7 Rating:
|
hello my question is what is the difference between S120 and S150 ? Please answer me I doubt that I choose the drive S 120 with the following configuration: -Active Line Module (+ Interface Module) -Line Connection Module -Motor Module -CU320-2DP or Select the drive S 150? My main issue is the ability to return energy Is the S 150 is designed adjust for a single motor and placed in a enclose ? no more difference between these two (S120 & S150)? |
Last edited by: Min_Moderator at: 9/23/2014 2:51 PMNew subject after splitting from /tf/WW/en/Posts/85669#top |
|
Follow us on