10/1/2014 3:27 PM | |
Joined: 10/11/2006 Last visit: 9/5/2025 Posts: 6038 Rating:
|
Hello, You can transfer the values for a traversing block with acyclic communicationusing the function block Sina_Para which is located in a library for Drives (EPOS): http://support.automation.siemens.com/WW/view/en/68034568 Please look also on the description located on this page. If you are running your positioning in MDI with continous transfer then every change of MDIposition / MDI speed etc is directly used in the EPOS and your axis should work without stopping - but this depends on your selected values. |
With best regards, |
|
Follow us on