5/19/2014 6:36 PM | |
Posts: 61 Rating:
|
Good day Please assist with parallel infeed. If 2 ALM are connected in parallel with one CU320, as per attachment. 1. How do I view status and parameters of individual ALM. 2.If AOP shows temperature trip, how would I know which one of the two is not cooling? AttachmentParallel Infeed1.pdf (143 Downloads) |
This contribution was helpful to
2 thankful Users |
5/21/2014 3:43 PM | |
Posts: 61 Rating:
|
Thanks for the response I don't have problem with configuration and setting up of the topology. The system is configured and working. Topology configured as per attachment My question is how do I see which of the 2 infeeds caused a fault, because on the AOP the faults is under infeeds not specifying which one of the two. I also could not find DO Number under the fault details on the AOP. Fault list appear as follows: 1: Control_Unit .............. ................... 2: Sub2_Infeeds Fault 3: TM31 .............. ..................... AttachmentParallel Infeed2.pdf (124 Downloads) |
10/29/2014 10:38 PM | |
Posts: 61 Rating:
|
Good day Could someone please assist with the solutionfor this problem. |
10/30/2014 8:09 AM | |
Joined: 4/3/2014 Last visit: 4/22/2025 Posts: 54 Rating:
|
I don't think you can see them indivisually, I'm facing the same issue. |
Follow us on