11/17/2014 8:00 PM | |
Joined: 4/9/2009 Last visit: 8/10/2025 Posts: 71 Rating:
|
Type text or a website address or translate a document. The situation is the following: - S7-1200 - KTP700 Basic PN 2nd generation The two elements are connected via Profinet and are programmed with TIA Portal V13 Upd6 (the last one - but the problem was the same with Upd3-4 and 5). In the design mode of the panel (WinCC Tia Portal Advanced) I have establish a certain order to the columns in the view of signaling (eg, number/date/time/status/text), but in both simulation mode and real panel, the order is different!!!! (eg number/time/status/text/date)! The project at design time shows the correct order while running is wrong. For sortingcolumns I make a double click with the shift on the object and then I drag the column to the desired position. It seems that the order of the columns is fixed and equal of the ticks that can be put in the object properties to select which columns to display. The same project in Tia Portal V12 work well. Siemens support has confirmed that is a bug of the V13. Do you have some workaround? Thanks and Best Regards |
7/12/2015 9:14 PM | |
Joined: 3/22/2014 Last visit: 8/22/2025 Posts: 102 Rating:
|
Also column ordering in trend object doesn't work in TIA V13 SP1 for this kind of panels.. |
Follow us on