10/24/2014 2:32 PM | |
Posts: 9 Rating:
|
Hey guys! So here's the deal. I've made a project in TIA portal V12 SP1 and then later on got to buy my self a PG M4 with V13 in it So then i thought, well let's make it to V13. Worst descision so far. I ended up with only some object visible no matter how I tried to configure the layers, transparent box marked, unmarked. Nothing works in my PG. Not even when i open the old V12 project in my PG. Can someone tell my what's wrong here? Isn't it supposed to use the transparentbox to make the objects backgroundcolor invisible, NOT the whole object? That function would be in logic called Invisible according to my opinion... Hope someone has a good answer to this, probably easier than I can think of. See my attached images. AttachmentWinCCV12V13.zip (342 Downloads) |
Last edited by: EricJacob11 at: 10/24/2014 2:36 PM |
|
10/28/2014 6:56 AM | |
Posts: 1299 Rating:
|
Hello, did you also change the image version to v13? Did you do "Compile > Software (rebuild all)" before starting the simulation? Sometimes there are also such display problems because of the windows settings: http://support.automation.siemens.com/WW/view/en/62052786 K!ke |
8/20/2015 11:48 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4760 Rating:
|
New question published by giunal is split to a separate thread with the subject Transfer old project V12 to new V13. Best regards |
Follow us on