10/2/2015 9:18 PM | |
Joined: 9/23/2005 Last visit: 9/10/2025 Posts: 4416 Rating:
|
“Simple Samples” are small projects that demonstrate simple features. The target is give a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps.
Description:
In this simple sample, it is possible to work with recipes (create, edit, upload, download), with the help of recipes and standard objects.
Requirements: WinCC Professional V13 SP1.
Project with a minimum configuration (stop button, tags, etc. - in this simple sample the WinCC already output values of a S7-1200 controller (PLC_Tag_1, PLC_Tag_2 and PLC_Tag_3 – they are the focus of recipe operation).
Configuration main steps:
References: Manual WinCC Professional V13.0 https://support.industry.siemens.com/cs/br/pt/view/92323076/en
Online helps system WinCC Professional V13.0 SP1 https://support.industry.siemens.com/cs/br/pt/view/109096785/en
FAQ Which VBS information and VBS programming tools are there in WinCC (TIA Portal)? https://support.industry.siemens.com/cs/br/pt/view/59885894/en
Tips and tricks for creating scripts in WinCC (TIA Portal) https://support.industry.siemens.com/cs/br/pt/view/57132412/en
Help → Visualize processes → Working with recipes → Examples (Basic Panels, Panels, RT Advanced)
Images: Due a size / format restrictions, the images are first compacted with 7z format (images.z7) and after that attached to a zip archive (data.zip).
Project: Due a size / format restrictions, the project are first compacted with 7z format (project.z7) and after that attached to a zip archive (data.zip). AttachmentData.zip (1057 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to
1 thankful Users |
Follow us on