12/11/2015 8:51 AM | |
Joined: 1/12/2007 Last visit: 4/10/2025 Posts: 40 Rating:
|
Hello All where i find CommandTable_Editor _v4.0 ? best regards |
12/11/2015 9:54 AM | |
Joined: 1/12/2007 Last visit: 4/10/2025 Posts: 40 Rating:
|
Dear william many thanks for your answere, you can see my problem on attached best regards Attachmentxx.pdf (111 Downloads) |
12/11/2015 11:41 AM | |
Joined: 1/12/2007 Last visit: 4/10/2025 Posts: 40 Rating:
|
you can see on ob1 net7 best regards Attachmentservo_surmex.rar (97 Downloads) |
12/11/2015 1:45 PM | |
Posts: 5225 Rating:
|
A piece of information that could have been helpful to mention: That library is for TIA V12 and you have TIA V13.0. So I need to guide you through the steps: 2. Go to the instructions drawer and change the version number to V3 (!) for the motion control. See the image from the previous post... so the V5 becomes V3 in my case. 3. Open the library (see above link) in the Libraries drawer - Global Libraries. The system asks to upgrade from V12 to V13 library... let it do that. 4. Drag the files meant for the PLC into the project (Master Copies: UDT and FB).. [target] 5. Create a Command Table technology function DB. 6. Drag the FB into OB1 and let TIA create a DB. 7. Drag the Command Table technology function DB as FB parameter. 6. Do a complete system compile. Handle errors if any. It may be needed to go inside the FB1 and update the data type (right click the red coloured data type name and set to update). Upgrade the motion version? 7. Go to the instructions drawer and change the version number from V3 to a higher version for the motion control. (my case is V5) The same idea as in step 2 but in reverse. 8. Do a complete compile. In my case there were errors. 9. Adapt the data types to suit the version number. 10. Do a final compile - This project can be used to build on or to copy the code out of. ----------------- See if you can follow the instructions. Else update you software (for free) to the current software version and use the attached project. Let us know if your issue is resolved. Good luck. AttachmentHMI_CommandTable_Editor_TIA13.1.zap13.zip (99 Downloads) |
Follow us on