12/22/2015 1:33 PM | |
Posts: 5225 Rating:
|
Ouch... no answer yet? ++ see attachment. |
This contribution was helpful to
1 thankful Users |
12/23/2015 12:54 PM | |
Posts: 28 Rating:
|
VERY THANKS WILLIAM UR LAST POST GAVE ME THE EXACT ANSWER I NEEDED.. |
1/11/2016 6:41 PM | |
Posts: 5225 Rating:
|
Hi there. The # and % goes to the notation that is used inside Step7 V1x. ..........................................................#myLocalVariable .........................................................."myGlobalVariable" ..........................................................%MW20
The problem with earlier TIA version was that the % was not included in the notation. Therefore it was possible to have #myValue.W1 and #myStructure.W1 where..
To reduce the possible confusion, Siemens included the % to indicate that the slicing method is employed on the variable. Go to the link above to learn about the different slicing methods that can be employed. w |
Last edited by: William_B at: 1/11/2016 6:42:30 PM |
|
Follow us on