5/19/2018 1:05 PM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello, Which OFF comands you have configured to STOP drive? In hoist or vertical application, motor holding brake should get open only when sufficient torque is generated in motor so that it will hold the load at position & will not allow it to drop. On the other side, motor brake should be closed at low rpm i.e. before the motor rests at zero speed which will prevent the load to fall down. So please refer the attached sheet which will help you to set motor holding brake open & close time/parameters. HTH. AttachmentMM440 motor holding brake .pdf (406 Downloads) |
5/20/2018 12:30 PM | |
Posts: 44 Rating:
|
Ok.Thanks |
Follow us on