3/27/2019 4:38 PM | |
Posts: 5 Rating:
|
Hello there: I have a problem that I have been trying to solve for days now. I have a DP slave ( 6ES7-151-1CA00-3BL0) which has 16 DI/DO, 4 AI, 2AI, and 2AI connected to it. The problem is all the inputs from this slave fails for ONE Second sporadically with the message below. ( S7$Dryer/@(2)/AS_Dryer_2 Read error I/O: FC105 Addr: 768 ) From my investigation, this error also comes when I disconnect Profibus cable from this slave. I check into the diagnostics of CPU and there are no sign of any failures but it is populate with Event ID : 16# A217. I have no clue what this A217 is. I would appreciate any help. Thank you! ------------------------------------------------------------------------------------------ |
Last edited by: Pi99 at: 3/27/2019 4:38:53 PMLast edited by: Jen_Moderator at: 3/28/2019 11:56:09 AMNew subject after splitting |
|
3/27/2019 4:48 PM | |
Joined: 9/21/2012 Last visit: 9/7/2025 Posts: 4704 Rating:
|
Don't post the same question twice! |
3/28/2019 11:57 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject Read Error is published within the conference Decentral Peripherie. Best regards Jen_Moderator |
Follow us on