8/12/2019 3:50 AM | |
Joined: 9/24/2014 Last visit: 6/24/2025 Posts: 1 Rating:
|
Good evening. I have exacty the same problem. My aplication is a hoist in a crane but the problem is the same. When I raise the full load it works but when I only hoist the wires load I get a F60036 fault. I answer the questions from Mr Mata with a trace of the parameters he ask for. This shows the operation from slow speed at half speed. Full speed is 1750 rpm. Does the speed oscillate around the set point? How much? I don't think so, see the trace, please. When no load operation, does the current set point oscillate between positive and negative values?I don't think so, see the trace, please. Wich isyour setting forKp (p50225) and Tn (p50226) of the speed loop? p50225=6.5 & p50226=0.5 Please can any expert help me with this issue. Best regards. AttachmentF60036.zip (411 Downloads) |
Last edited by: CBou at: 08/12/2019 03:50:40 |
|
Follow us on