6/9/2016 6:10 PM | |
Posts: 4 Rating:
|
Hello, I am trying to control my motor with motordrive s110 Cu305 PN. I took the necessary steps to connect and the connection is working. We imported the drive libraries into tia portal. Both are version 13. We are trying to use FB284 (sinA_pos) to position or motor using tia portal. The problem is I don't really understand which parameters I need to adjust. I am basing myself on the following document: https://support.industry.siemens.com/cs/attachments/109475044/SINAMICS_Blocks_TIAP_V12SP1_V13.pdf In the attached zipfile you can find 2 pictures of how I implemented the function block in my OB1. The way I understand it, the motor should start moving when i push the button attached to I0.3. On the LADDR entrances I use Telegram111. Our LU is equal to 0,1mm by using STARTER. Is there anything else I should do before the motor should start moving? Or is this a wrong way to implement the function block in OB1? Thank you, Bert AttachmentFB284.zip (1097 Downloads) |
Last edited by: Min_Moderator at: 6/10/2016 1:28:54 PMEdit link |
|
6/10/2016 12:31 PM | |
Posts: 4 Rating:
|
Here are some extra pictures. When we monitor our values in the Data Block we see that we get an error and the warnact gets the value 16#1D2C. We can't find what this warnact means. Kind regards, Bert AttachmentFB284 10-06.zip (792 Downloads) |
This contribution was helpful to
1 thankful Users |
6/21/2016 10:52 AM | |
Posts: 14 Rating:
|
Hi Bert_VE I'm working on a s120 and i have to use a block fb284 too. Is that you who have created the block or we can found the block in a library? Thanks |
8/27/2019 1:53 PM | |
Joined: 3/2/2015 Last visit: 9/5/2025 Posts: 67 Rating:
|
Documentation for FB284 and FB285 is located on below link https://support.industry.siemens.com/cs/af/en/view/109475044 |
Last edited by: Jen_Moderator at: 08/27/2019 14:35:33Optimized link. |
|
Follow us on