12/9/2019 10:39 AM | |
Joined: 9/3/2013 Last visit: 9/10/2025 Posts: 152 Rating:
|
Hello HAMEE, this question isns't easy to answer. The basic values of the Communication resources of the CPU 410-5H can you find here: https://support.industry.siemens.com/cs/de/en/pv/6ES7410-5HX08-0AB0/td?dl=en part: Communication functions e.g. Number of connections However, there are other factors: E.g. Do you want to use fault-tolerant S7 connections. See: 17.11.2 https://support.industry.siemens.com/cs/de/en/view/109748473 In addition, it should be clarified how much data should be transmitted per AS-AS connection. Best Regards |
This contribution was helpful to
1 thankful Users |
12/18/2019 7:31 AM | |
Joined: 5/3/2017 Last visit: 2/6/2025 Posts: 673 Rating:
|
Hello HAMEEE, you can find the recommendation from Siemens for the transmitted data per AS-wide interconnections in the manual PCS 7 Compendium Part A - Configuration Guidelines at the section AS resource utilization. With regards |
This contribution was helpful to
1 thankful Users |
Follow us on