1/19/2020 6:29 AM | |
Posts: 110 Rating:
|
Hi What is the function Of this Push Switch in NCU Cards, Rana Ali |
1/19/2020 9:28 AM | |
Posts: 110 Rating:
|
Hi Sir Iread this topic in wiki site Incomputing, anon-maskable interrupt(NMI) is a hardwareinterruptthat standard interrupt-masking techniques in the system cannot ignore. It typically occurs to signal attention for non-recoverable hardwareerrors. (Some NMIs may be masked, but only by using proprietary methods specific to the particular NMI.) An NMI is often used when response time is critical or when an interrupt should never be disabled during normal system operation. Such uses include reporting non-recoverable hardware errors, system debugging and profiling, and handling of special cases like system resets. Moderncomputer architecturestypically use NMIs to handle non-recoverable errors which need immediate attention. Therefore, such interrupts should not be masked in the normal operation of the system. These errors include non-recoverable internal systemchipseterrors, corruption in system memory such asparityandECCerrors, and data corruption detected on system and peripheral buses. On some systems, a computer user can trigger an NMI through hardware and softwaredebugginginterfaces and system reset buttons. Programmers typically use debugging NMIs to diagnose and fix faulty code. In such cases an NMI can execute aninterrupt handlerthat transfers control to a special monitor program. From this program a developer can inspect the machine's memory and examine the internal state of the program at the instant of its interruption. This also allows the debugging or diagnosing of computers which appearhung. But in NCU whiches type intrreupt or when we push or used excuatly this push switch, Rana Ali |
Follow us on