12/24/2008 3:27 PM | |
Joined: 4/6/2006 Last visit: 6/24/2025 Posts: 604 Rating:
|
Hello Darius, The license you need depends on the type of connection you use. So you use SOFTNET you don't need the hardnet licenses (Only necessary when using a special CP like CP5613, CP1623, etc.) Everything below is based on SIMATIC NET 2008. Profibus: SOFTNET S7: 6GK1704-5CW71-3AA0 S7 Communication over ProfiBus SOFTNET-DP: 6GK1704-5DW71-3AA0 SOFTNET-DP Slave: 6GK1704-5SW71-3AA0
Max. 64 Connections Max.8 Connections |
Best regards, |
|
This contribution was helpful to
2 thankful Users |
Follow us on