7/28/2020 8:31 AM | |
Joined: 6/14/2018 Last visit: 7/4/2025 Posts: 4 Rating:
|
Hi, As per your attachment in the last step when configuration is pressed then encoder configuration effective option are coming. The used second encoder in my case is 6FX2001-2CC50 (see attachment for encoder details). So, my doubt is which bit to select & which to deselect. Second encoder is with SMC30. Can u plz write about axis md data with internal encoder bypassed only external active. Also should I make any changes in drive md for One more doubt, should I write DB3802.DBX1.6 in PLC to set second encoder active?.Because in PLC of spindle axis only DB3802.DBX1.5 is written. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/28/2020 10:58:11New subject after splitting |
|
7/29/2020 1:57 PM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
User can not bypass inetrnal i.e. motor encoder & active external encoder. Motor encoder is used for position as well as velocity feedback. Only external encoder can be bypassed & motor encoder can be set for position feedback. HTH HTH. |
This contribution was helpful to
1 thankful Users |
7/30/2020 10:15 AM | |
Joined: 6/14/2018 Last visit: 7/4/2025 Posts: 4 Rating:
|
Dear PISCEAN 2010, Sir thank u for ur reply.I am not bypassing internal of linear axes (i.e x & z), I have bypassed spindle axis internal encoder (in this case simple turning is running but threading is not happening) & my machine is working ok. But for threading I want to active only external encoder of Spindle. For this I have attached last step of encoder configuration about bit selection. Plz suggest, I already let u know about encoder details & also smc30 in the previous post. |
8/1/2020 12:59 PM | |
Joined: 6/14/2018 Last visit: 7/4/2025 Posts: 4 Rating:
|
Hi PISCEAN 2010, Thanks for the support. I have solved the problem. |
This contribution was helpful to
1 thankful Users |
Follow us on