1/12/2009 2:36 PM | |
Joined: 9/27/2006 Last visit: 9/7/2025 Posts: 12401 Rating:
|
Hello sh.m; If you are using Profibus-DP slaves. and one of the slavesis an ET 200S, you could add a1SI ("single serial interface") module on the ET 200S and use that as a Modbus master. If you already have the ET 200S platform then this is a very cheap and efficient alternative. If interested, you can look at the chapter on Modbus in the following 1SI manual: http://support.automation.siemens.com/WW/view/en/9260793 Another option could be a Profibus-DP master to Modbus RTU master gateway. Look at fieldserver.com or prolinx gateways (prosoft-technology.com) for typical examples. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 1/12/2009 4:55 PM |
|
Follow us on